Other Parts Discussed in Thread: TX7316
Hi
I have a TX7316 Evaluation Board which i have setup in 3-level mode. When i run it in on-chip mode it has limited number of transitions(16)
allowed for pattern profile of a pulse. Basically i am interested in sending a chirp with quite a lot of cycles which is not possible i believe using on chip.
So i was wondering if i can run the off chip mode on that evaluation board using J11 Connector and if yes, what are the hardware changes i need to
perform to make it work. It says it has IN control signals connected to ground when in on-chip mode.
User guide doesn't describe much about off chip(just some switches in action) If i run off chip, does it mean i can directly talk with CPLD using
jtag connector.