Hi I am using FMC150 card having ADS62p49 on a Xilinx ZC706 board LPC connector. I have provided 10 MHz input and when i see the samples coming out of ADC on ILA of Xilinx, the digital output is sine wave but the amplitude of sine wave is also sinosuidally varying. My registers are set for CMOS type output with Low Speed enabled as I am sampling at 61MSPS.
The pin layout for FMC150 shows only pins of ADS62p49 as _N and _P (For ex CH02_N,CH02_P,CH04_N... 7 such pairs) type LVDS configuration but I am using the ADC with LVCMOS Outputs. Can someone suggest how _N and _P are connected with 14 bits of ADC.