Hi Team,
We have customer inquiries regarding the document "An Efficient Power Supply Reference Design for Optimizing Spur and Phase Noise in RF-Sampling DAC" in the given link below:
1. Figure 6 is described as showing spur suppression (dBc I assume) versus ripple frequency, but the axis is labeled as ripple voltage (mV pk-pk) versus ripple frequency. Is the former information available?
2. Graphs showing spur suppression versus RF output frequency are shown for only three supplies (VDDCLK1, VDDA1, & VDDPLL1). Is there any information on the other clocking and analog supplies? Particularly if some of them are as sensitive to ripple as VDDCLK1. I'm assuming ripple on digital supplies has no effect, as long as it's not very high (>50mV), but confirmation would be nice.
3. How was the DAC configured for these tests (one or two TX, sampling rate, interpolation)?
4. Is there any information on the spurious performance up to 4.5GHz RF output?
let me know if you need more information from the customer.
Thanks!
Jonathan