Hi E2E,
Good day.
We have one customer asking for the ESD classification and or rating for DAC7568.
Information is not available on the datasheet. Appreciate it if you could help to provide.
Thanks in advance!
Art
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi E2E,
Good day.
We have one customer asking for the ESD classification and or rating for DAC7568.
Information is not available on the datasheet. Appreciate it if you could help to provide.
Thanks in advance!
Art
Hi Art,
Thank you for your query. I am checking internally. I should be able to provide the information on Monday.
Regards,
Uttam Sahu
applicatiojns Engineer, Precision DAC
Hi Art,
Sorry for the delay. Please find below the details:
Test Type |
Precondition |
Test Condition |
ESD - HBM |
0000 |
2500 V |
ESD - MM |
0000 |
200 V |
ESD - CDM |
0000 |
1000 V |
Hope that answers your question.
Regards,
Uttam