This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 262
Part Number: ADS8688A
Dear team,
I am testing our ADS8688A EVM and my input signal is a DC voltage from 0V to 5V.
Use the input range of 0~5.12V,
connect the OPA2209 filter between input DC signal and ADC input pin. then the ADC output error is extremely larger: 2V DC Vin, ADC output 1.698V, as shown in following picture.
Here is some test results during debug.
The voltage in A0+ of J25 is 2V DC, but voltage in J8 pin is 1.69V, so the ADC input pin voltage is 1.69V.
So I think this error between 2V and 1.69V ADC output is come from OPA2209 circuit, but this is only a 2nd order LPF.
Can you give me some help on this issue? Thank you!
Best regards
Yunjing
Duplicate thread.
Please see
In reply to Cynthia:
Neither of the two thread get useful answer. Please help on one of this two question.
Thank you !
In reply to Yunjing Wang1:
Hello
Apologies for the late response and confusion due to the duplicate post
The OPA2209 is a second order filter with a cut off of 22Khz, thus the DC input should be able to pass through.
Were no components on the board changed previously?
This filter is also available for channels 0-3. Would you test this other channels to see if the DC input is also attenuated?
Regards
Cynthia