Part Number: ADS8638
Hi,
There is an issue about the accuracy of ADS8638. The failure percentage is 40%.
Input : DC 5V from power supply to AIN0-7 => Output value 0-7: 5.012V
Input : DC 0V from power supply to AIN0-7 => Output value 0-7: 12mV
Is this related to input offset voltage ? Is it any possible to improve this issue by software or hardward ?
Jackson