Hi ADC Experts!
My customer is running into challenges that the input channels to the ADS7952 are seeing a voltage drop compared to the expected divided down voltage.
How much current do we expect to see drawn into the ADS7952 inputs when the input is switched on?
Setup:
VBD=VA=3.3V
CH7 connected to 5V with 30.1kohm and 20kohm divider
VREF = 2.5V
No PGA connected between MX0 and AINP.
Thanks!
Reed