Part Number: ADS1292
Other Parts Discussed in Thread: OPA2188, INA828
Hello
I would like to ask a question to be sure ,
does adding an external buffer opamp with hight CMRR would increase the ADS1292 CMRR performance ? ( one lead ECG no RLD)
OPA2188 has a very good high CMRR 146dB .
do in this case still need RLD ?
DC bock Capacitors ?
does the supply voltage effect the CMRR of OA2188? for for example -/+ 5V is better than -/+2,5V ? or same?
I am sorry to ask much , Thank you in advanced