Other Parts Discussed in Thread: ADS1299
Hello,
I'm starting using the ADS1299 Performance Demonstration Kit which is composed by the MMB0 board and the ADS1299EEG.
I received the box with these two components and without a specific power supply. The section 2.4 of the user manual mention (slau443b) that the kit includes only these two parts.
Very strangerly I found in the manual the first sentence of the paragraph 3.3 which says:
Apply power to the MMB0 using the supplied wall mount power supply and connect the MMB0 to your PC
via any available USB port.
Why this sentence refers to a supplied power supply? It is quite confusing!
Anyhow, reading the specifications of the power supply on the manual I put a 6V - 1A commercial wall mount power supply in the main jack input after having controlled the proper polarity.
The boards don't start and, while the board is connected to the power supply, the input voltage drops to 2V. After removing the connection the input power supply continues to work.
Do you have any idea that would help me to work with the boards?
Please let me know if I can consider the board failing or if some further test are needed.
Thank you in advance,
BR,
Gionatan