Other Parts Discussed in Thread: REF5025, REF5020
Hi,
I have a question about ADS131A0x working with external reference voltage source. I use currently the ADS131A0x with negative charge pump enabled and my AVSS is tied to analog ground of the circuit. I need to change the design slightly and I am modifying the design to work without charge pump, AVDD connected to 2.5 V and AVSS to -2.5 V.
- The modification on pin 11 is necessary and clear
- AVDD pin 9 is decoupled to AVSS on the device terminal.
- I got confused with the reference source. On page 31 of datasheet it is recommended to refer the reference source to AVSS which is now -2.5 V not GND. Also, the input voltage to the REF5025 is just 3.3 V with respect to GND. How should I understand it? I was sure I can keep the external Vref without any change (as 2.5 V with respect to GND) and provide it to ADC as previously referenced to ground. I attach recommended configuration below.
I will appreciate Your input.