hi,
CTM has used LMP90080-Q1 in system. But they have met some application problem. the details as follow.
A The Part of Schematic
B Problem description
1 SPI communication is OK, and the configuration gain is also good. When reading data, the channel is misplaced.
For example, the input of CH0 is displayed in CH1, and the input of CH1 is displayed in CH2.
2 The description of several sampling modes in datasheet is not very detailed. The situation is the same as that described in description1 when we change the sampling mode.
3 Please provide the main registers needed to be configured and the configuration examples.
The specific problems are as follows:
1) The test overview and configuration picture.
Initialization configuration
Configuration of each channel
CH1 connected to thermistor
2) Configure as 4CH test mode, the test result is as shown in the figure, N-type thermistor is connected to CH1, but the test data is shown in CH2
3) Configure it as a single channel test mode, Remove the other three channels. There is no problem with the test data. The value is shown in CH1.
Touch the thermistor by hand, and the data will be displayed in CH1 correctly.
May I get your swift support? thanks.
BRs