Other Parts Discussed in Thread: DAC53608
What the load current can be bear from 0V to Vout when VDD=3.3V?
Do you have the test data or plot to describe it ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The Electrical Characteristics Table indicates that the specifications were collected with VDD from 2.7V to 5.5V. As such, the table applies to your requested case of 3.3V VDD.
On page 8 you will find the DC output impedance. This applies to the entire linear region of operation. What would be considered linear depends on the relationship of VDD and VREF in your system.
Hi Jericho,
The DAC80508 and DAC53608 can both drive 6mA into a load. This should not be a problem for either.
Thanks,
Paul