Other Parts Discussed in Thread: TPS793
Hello,
I'm using an ADS124s08 which is connected to an MCU. The application requires it to sample data pretty rarely, therefore, for the rest of the time I would like to reduce the power consumption.
One of the higher current sinks in the system are the resistive bridges I'm sampling with the ADC and I realized that the AVSS-SW pin of the device is made for that. However, the hardware is not configured for using it (the low side power of the cells is not taken from AVSS-SW pin).
In contrast, the analog section of the system is powered through a dedicated LDO (TPS793), which have the ENABLE pin that I can control from the MCU.
The question is: can I safety turn off the analog power to reduce the consumption of the bridges? Is so, does the DRY flag of the STATUS register properly indicates when the analog part has ramped up?
Thank you,
Davide