Hi,
I have two DAC38RF80EVM boards and two TSW14J56EVM boards. How can I set them up so that they can generate phase synchronized signals?
Thanks,
Steve
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have two DAC38RF80EVM boards and two TSW14J56EVM boards. How can I set them up so that they can generate phase synchronized signals?
Thanks,
Steve
I actually would like to achieve the following:
Case 1) Use an external DAC clk, split the clock to two DAC38RF80EVMs and trigger the waveform generation using an external trigger signal provided to J13 on both TSW14J56EVM.
Case 2) Use internal PPL generated DAC clk on one DAC38RF80EVM, and provide that to the second DAC38RF80EVM. And then trigger the waveform generation using an external trigger signal provided to J13 on both TSW14J56EVM.
Hi Steve,
We are looking at your question and will get back to you soon.
Regards,
Neeraj
Hi,
I tried to set up the two boards with two TSW14J56EVMs and provided a hardware trigger to both boards. It seems both DACs are triggered when J13 sees a rising edge. I actually was expecting the DAC would only be active when J13 is HIGH. Is there a way to modify the setting?
Thanks,
Steve