Hi,
I would like to use a DAC output > 2.5V internal VREF, so I disabled reference divider, and enabled GAIN to accomplish this (GAIN REFDIV-EN = 0, BUFFx-GAIN = 1). I only had VDD = 3.3V since this is the max value I need. I expect that value < 3.3V should be allowable, and maybe clamp at 3.3V if Iset a value that will exceed this; but DAC output is always at 0V when I try various values below 3.3V.
Playing around the settings, any setting with REFDIV-EN = 0 does not any output at DAC:
- REFDIV-EN = 1, BUFFx-GAIN = 1, DAC output is set as expected.
- REFDIV-EN = 1, BUFFx-GAIN = 0, DAC output is set as expected.
- REFDIV-EN = 0, BUFFx-GAIN = 1, DAC output is always 0V.
- REFDIV-EN = 0, BUFFx-GAIN = 0, DAC output is always 0V.
Anything I could look at to make REFDIV-EN = 0 to work? Thanks!