Hi there,
we were lucky when we measured an external current via the Current Sense Pins and a shunt (200mR). Under roomtemperature it seems to work.
But then we tried to measure that same current under hot temperatures up to Tambient=125°C and had a massive shift in the reading value vs. the reallity. The current reading from the AMC told us a value which was almost as double as high as the reality was! We have seen a wrong temperature reading from around 50°C on...
So again - the AMC is telling us a too high temperature so he thinks the differental voltage across the shunt (200mR) is higher then it is.
Shunt is specified up to 175°C.
Thermalpad of AMC is on Vss not on GND. The AMC is working under 125°C (SPI working, bipolar DAC driver are working).
So not sure if the AMC has a thermal problem? But what is against this thesis is (SPI, DAC working, shift already from lower temperatures...).
Do u have any idea what it could be?
Thanks,
Markus