Other Parts Discussed in Thread: ADS1294
Hello.
Thank you for answering.
(1)The figure in the ADS1294 datasheet is correct. I will make a note to have this changed.
→I understood.
(2)There is no issue or change in characteristics when using DVDD = 3.3V as opposed to 1.8V.
→I understood.
(3)With DVDD = 0V, I would expect no response from the device, regardless of what is on the inputs. Please see the "Data Format" section for additional information.
→Sorry, DGND=0(V) instead of DVDD=0(V).Correct the question as follows.
(Q.)
[Power Supply AVDD: +1.5(V), AVSS: -1.5(V), DVDD: +3.3(V)]
[External References: VREFN = AVSS, VREFP - VREFN = +2.5(V)]
In the case of AINN=DGND=0(V), Gain=1, will VREF, input-signal VIN, Full-Scale-Range, VIN range, ADC-Code be as follows?
・VREF=VREFP-VREFN=+2.5(V)
・VIN=AINP-AINN=AINP
・Full-Scale-Range=5(V)
・VIN range: -2.5(V) ~ +2.5(V)
・ADC-Code
(VIN : ADC-Code)
> +2.5(V) : 7FFF
+2.5/32767(V) : 0001
0(V) : 0000
-2.5/32767(V) : FFFF
<-2.5/(32768/32767)(V) : 8000