Dear colleague,
Our customer encountered below issue:
Operation steps:
1. After power on, send RESET signal (low level) to DDC264, reset is normal; After reset, start register configuration.
2. Send configuration information(FORMAT=1, Set 16Bit output, send "0010 0000 1000 0000"), then DDC264 return “30F066012480F6h”, it meets the datasheet description.
3. Send CONV signal, after signal changes, DDC264 doesn't return DVALID signal, so no DOUT signal.
Control logic is as below:
Is there any problem with the above configuration and control of DDC264? Why there is no DVALID signal?
Thanks a lot!
Best Regards,
Rock Su