Hello.
ADS 1198 and ADS 1194 are used as 12 channels in "Standard Mode (Use CS1 and CS2)".
If I don't use the RLD, is the connection as attached document?RLD CONNECTION.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.
ADS 1198 and ADS 1194 are used as 12 channels in "Standard Mode (Use CS1 and CS2)".
If I don't use the RLD, is the connection as attached document?RLD CONNECTION.pdf
Hi,
The only change I suggest is to tie RLDREF to AVDD as well. The RC can be left open.
Make sure to keep the RLD buffer disabled in the register settings to save power.
Thank you, Alexander Smith.
Changing RLDREF to AVDD is difficult (already made PWB).
If there is no problem with the operation, I would like to keep it open, but is there any problem?
Set RC to OPEN.
RLD buffer is Power-Down (Config3: PD_RLD = 0 (Default)).
Hi,
I do not think it will damage the device. You may see a slight increase in dissipated power.
Hello, Alex Smith.
I leave open if there is no damage or malfunction.
Is there any problem other than increasing power consumption?