Other Parts Discussed in Thread: REF5045,
In the data sheet it states :-
"Select RREF_FLT and CREF_FLT to limit the broadband noise contribution from the external reference source. The device takes very little current, IREF, from the REFIN pin (typically, 0.1 μA). However, this current flows through RREF_FLT and may result in additional gain error."
I am using the REF5045IDGK as my external reference and I have placed it very close to the ADS8900BRGE pin 3. I have also connected 2 x 10uF 10V 0402 X5R Caps on this track. Is this additional RREF_FLT and CREF_FLT required ? It does not appear to be mentioned in the REF5045IDGK data sheet ? Also "However, this current flows through RREF_FLT and may result in additional gain error." - does this mean that there is a preference not to place the RREF_FLT ?
Thank you in advanced