Hi,
I am trying to use ADS1259 EVM patch board in the standalone mode.
For writing my own Master I have captured the initialize procedure data coming on SPI ports.
I have observe that for each input command byte is followed by the some unexpected byte on the output port.
The first command byte on DIN input is 11H i.e. SDATAC with 00H on the DOUT port.
The secomd command byte on DIN input is 0AH i.e. STOP with 02H on the DOUT port.
similarly third input byte is 06H with 1DH on the DOUT port.
This behaviour is not given in the datasheet. Is this the response from the device to the input command sent ?
If yes, what is the response for the other commands of the ADS1259 ?
Regards
Husain Asif