Hi there,
have several AMCs on my board and already using them as expected. But one of them is working differently and not sure if it is damaged or what I can do.
Normally when the AMC is clamping it goes with the DAC bipolar to -5V. But at one AMC (only one of that DAC pairs) is Always going to around 0V instead. So AVss -5V is working properly cause the 2nd bipolar DAC seems to work and clamping.
The DAC itself is also working when I write the Register...I can set around -5...0V manually via SPI. So it seems it is electrically capable. But only when it gets a clamping command...it`s not.
Thanks and regards,
Markus