Hi,
I've narrowed our part selection down to ADS8900B and AD4020. The AD4020 specifies the 0.1Hz to 10Hz noise at ~6uV-pp. Do you have any 1/f noise data to share for the ADS8900B? Or, suggest a method I can measure it on the evaluation kit?
In addition, if we use 2.5V reference instead of 5V, can we expect to see 2x lower noise floor overall? I understand if we are trying to run full scale swing, the SNR would not improve, but our signal is so small I'm thinking to go with a low reference to reduce noise further.
Thank you!
Erik