This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8881: They are looking for a ADC device which can start sampling data and conversion after one timing signal input. Do you know such device?

Part Number: ADS8881
Other Parts Discussed in Thread: ADS127L01

 Hello guys,

 One of my cutomers is looking for a ADC device which can start sampling data and conversion after one pulse input.

 Their requests spec for the ADC are the follows.

1. 18bit. 

2. 500kSPS.

3. INL=+/-1.5dB.

4. 1 channel differential input.

5. SPI IF

6.  AD converter that starts sampling and converts after that when one timing signal is input.

 Do you have any ADC device which can be suited for the above?

 Your reply would be much appreciated.

 Best regards,

 Kazuya. 

  • Hello Kazuya-san,

    The ADS8881 has a separate CONVST pin which starts the conversion process, so I do think it meets the above requirements.

    However, are you asking for a device that will start conversions with one timing signal input, and then continue to convert at 500ksps without additional timing signal input?

    If this is the case, the only 18b+ devices that continuously converts and can be synchronized to an external timing event are the delta-sigma ADC's.

    The ADS127L01 may work in this case, but has an internal digital filter that takes 5 samples to fully settle to a step input.

    Regards,
    Keith Nicholas
    Precision ADC Applications

  •  Hello Keith,

     Thank you very much for your reply and I'm sorry to be my response.

     I told the device you recommended to the customer.

     Thank you again and best regards,

     Kazuya Nakai.