Other Parts Discussed in Thread: ADS124S08,
I'm using K-type thermocouple to measure temperature which connected between AIN0 and AIN1 of ADS112. Section 9.2.1.2 Detailed Design Procedure in datasheet describes algorithm that should
be implemented on the microcontroller to compensate for the cold-junction temperature. So according to 1st step, I need to measure the thermocouple voltage between AIN0 and AIN1 (I have configured registers accordingly). Whatever 2 bytes of data I read manualy/automatically, is it in Volt or milivolt? I want to make sure that translation (using NIST table) of summation of Vtc(thermocouple voltage) and Vcj(translation of temperature measured in device internal temperature sensor mode) gives an actual temperature.