I want to have the ADC converting autonomously and alerting me when the values are outside the window I set up, but I also want to be able to read it periodically.
Looking at the diagram in the datasheet (Figure 57. Configuring Device in Autonomous Mode), it appears I need to set it for "Pre-Alert" mode and then set the "Seq_Star" bit.
If I want to read it when it has not generated an alert, do I then set the "Seq_Abort" bit? Or can I just read the register?
It also indicates reading the data from the data buffer. In the register addresses, it only indicates the Ch0 & Ch1 accumulated data register. Is this the correct data register to read, even if I am not using the accumulator function?