Other Parts Discussed in Thread: ADS54J64, ADS54J66EVM
Hi,
I'm considering buying a ADS54J64EVM board, to be used directly with a KC705 and possibly a third-party JESD204B IP core for high-speed data acquisition and processing, but I have a few questions:
A) Are the boards compatible? From what I saw in the schematics for the ADS54J64EVM it seems so, but I would like to be sure before buying (and I'm not particularly familiar with JESD204 yet). I understand that the KC705 has a limited number of high-speed transceivers available on the FMC HPC connector, which can pose a problem.
B) If they can be connected, would I be able to use all the features of the ADS54J64 (eg. all 4 channels)? If not, which features would I lose?
C) What kind of support (in the form of example projects, code and IP cores) is provided for this kind of setup?
Best Regards,
Laez