This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32RF45: Matching Input Impedance to 50 Ohm

Part Number: ADC32RF45

Good day,

We are using the ADC32RF45 on one of our boards (sampling at 3 GSPS). We are using the input drive circuit of Figure 239 in the ADC32R45 datasheet (SBAS747C), except we do not have the optional 5 Ohm series resistors (causes too much attenuation) and we also do not have the resistors between the two transformers. However, we do use the TC1-1-43 as suggested and the coupling capacitors.

At high frequencies (1.42 GHz - 2.75 GHz), we are missing SFDR datasheet performance by more than 10 dB. According to Figure 63 in the datasheet, the input resistance is very low, 20 Ohm, at these high frequencies. We assume that we are getting bad performance due to impedance mismatch.

Does TI provide a method/advice of matching the low input impedance at these frequencies closer to 50 Ohm without introducing too much attenuation in the input drive circuit.

Kind regards,
Francois