Any difference between using the ADS1263 and ADS1262?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Dale,
The ADS1263 is basically the same as the ADS1262 except that there is an additional 24-bit ADC. Based on your early question regarding strain gauges, I'm guessing you are considering the ADS1262/63 because of 32-bits. Although the ADC can resolve to 32-bits, this doesn't mean you can actually achieve all 32-bits in the measurement result as noise will be a factor. Noise can be a result of external influences as well as the noise of conversion. For strain or load cell measurements you want to consider a stable, or noise-free, result. For your application you may want to consider the ADS1235 or the ADS1260. Both of these devices are low-noise 24-bit ADCs that offer good levels of performance.
Best regards,
Bob B