This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] ADS1258: ADS1258 and ADS1258-EP Thermal Information

Guru 50440 points

Replies: 1

Views: 176

Part Number: ADS1258

The thermal information for the ADS1258 and ADS1258-EP is not in the datasheet.  Is this information available?

Regards,
Collin Wells
Precision ADC Applications

  • Please find the thermal information for the ADS1258 and ADS1258-EP for the two packages below:

    VQFN (RTC) Package:

    Result- Theta JA-High K (standard datasheet value) 27.1
    Result-Theta JC, top (standard datasheet value) 18
    Result-Theta JB (standard datasheet value) 11.6
    Result- Psi JT (standard datasheet value) 0.3
    Result- Psi JB (standard datasheet value) 11.6
    Result-Theta JC, bottom (standard datasheet value) 4.4


    HTQFP (PHP) Package:

    Result- Theta JA-High K (standard datasheet value) 31.5
    Result-Theta JC, top (standard datasheet value) 22.5
    Result-Theta JB (standard datasheet value) 15.0
    Result- Psi JT (standard datasheet value) 0.5
    Result- Psi JB (standard datasheet value) 15.0
    Result-Theta JC, bottom (standard datasheet value) 6.5

    Regards,
    Collin Wells
    Precision ADC Applications

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.