Other Parts Discussed in Thread: ADS1115
Hi,
The ADS1118 data sheet (p.30) states that AIN0, AIN1, and AIN2 can be measured with respect to AIN3. What is the recommended input filtering option in this case?
Also, the data sheet mentions that this configuration doesn't offer common-mode noise attenuation. However, the selected inputs (for example, AIN0/AIN3 or AIN1/AIN3) are stil subtracted, i.e., the ADC processes the differential signal. It seems that common-mode signal disturbance will be canceled out. Could you clarify?
Finally, comparing ADS1118 with ADS1115, it seems they use the same ADC core with different digital interface (SPI vs. I2C). Fig 2 in the ADS1118 data sheet and Fig 19 in the ADS1115 data sheet both show total error vs input signal -- but although they look similar in shape, one has error scale in millivolts while the other one in microvolts. Is this a typo? I imagine the mV version is correct?
Thanks!