Part Number: ADS1292R
Dear TI experts:
Hi, I'm designing a wearable sensor for ECG detection.
I want to measure 2-electrode ECG and respiration without a third electrode.
I connected RLDOUT after the input ac-coupling capacitors with resistors to cancel common-mode voltage.
Here is my schematic:
1. Because this device is battery operated, I don't care to 60 Hz noise. So, I set the high-pass filter cutoff to 10 Hz. Is it correct?
2. In the datasheet, the low-pass filter already exists in front of the ADC. Is it necessary to put RC filter in the signal path to IN2P and IN2N?
3. In AC coupled applications, is the patient protect resistor really required? I want to save passive components.
4. How to choose capacitance of C18 between 47 nF and 4.7 nF?
Best regards,