Hi
In the datasheet the analog voltage the absolute min is -0,3 V and absolute max is 6 V.
The Nominal analog votage is 5 V.
I use this setup with 5 V already in an application.
Now I want to use it in another application but here I only have 3,3 V available.
Can I use the ADS7253 with 3,3 V as analog voltage?
BR
Magnus