I am seeing no output (0 V regardless of code setting) from DAC60501.
Vcc is 3.25 V (measured) and VREF output is 2.5 V (measured).
The REF-ALARM bit in the STATUS register is reading as 1. The datasheet says this bit "reads 1 when the difference between the reference and supply pins is below a minimum analog threshold.Reads 0 otherwise."
I don't find that the minimum analog threshold is specified in the datasheet. What is the minimum Vcc to avoid this condition? Are there any other conditions that can cause the REF-ALARM bit to be set? What settings can be used to get a non-zero output from the DAC?
Other observations:
* Register 01h reads as 2195h. This doesn't match the datasheet spec which says field [11:8] should be 4 rather than 1.
* I see the REF-ALARM bit set for all settings of the REF-DIV and BUF-GAIN bits.
Thanks,
Matt