Part Number: ADS1261EVM
Other Parts Discussed in Thread: ADS1261
Hi,
In the ADS1261 EVM datasheet (section 9.3.6) it specifies using the IMUX1 and IMUX2 registers to connect the corresponding current sources to the analog inputs, and then specifies using IMAG1 and IMAG2 to set the corresponding current magnitude. Immediately thereafter it says "Enable the internal reference for current source operation".
I've looked through the registers (particularly the REF register) and don't see how to change the internal reference functionality. I'm testing the sensor-excitation current source with a 100Ohm resistor across AIN1 and AIN0 (with IMUX1 set to AIN1 and IMAG1 set to 100uA). I expect to see 10mV on scope probes that I place across the resistor, yet I see nothing. How do I configure the internal reference for current source operation?
Regards,
-Adrian