This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 103
Part Number: ADS9224R
Hello guys,
One of my customers is looking for a A/D converter which can be connected to a controller with Dual/Quad SPI interface.
Can ADS9224R be used with Dual SPI mode or Qual SPI mode?
If the answer is No, could you please give me any TI ADC device which can be used with Dual/Quad SPI interface.
Your reply would be much appreciated.
Kazuya.
Hello,
Yes, the ADS9224 has a multi-SPI mode that TI calls "Enhanced SPI" (or sometimes multi-SPI on older devices that have the feature). Please read through the datasheet sections on the enhanced SPI information and let us know if you need additional information.
Some of the other higher throughput, higher resolution devices, like the ADS8900B also offer this type of interface.
Regards,Collin WellsPrecision ADC Applications
In reply to Collin Wells:
Hello Colin,
Thank you very much for your reply.
I understood.
This interface is the first trial for the customer to use. They need any reference design or technical document about TI enhanced SPI
to understand the SPI usage. I found the following document as one of them.
Simplify Isolation Designs Using an Enhanced-SPI ADC Interface.
http://www.ti.com/lit/an/sbaa241/sbaa241.pdf?&ts=1589776507601
Do you have any document to understand for TI enhanced SPI protocol and connection between controller and device, etc?
Thank you and best regards,
Kazuya Nakai.
In reply to Kazuya Nakai59:
Hello Nakai-san,
There are no documents specifically for the enhanced SPI in the ADS9224R, but we can help your customer configure the device for their application. Could you tell us some key parameters, such as desired data rate and SCLK frequency?
If they have any specific questions about the mode offerings, I can help to clarify those directly.
Best regards,
Ryan Andrews
Applications Engineer | Precision ADCs
Are you working on a bio-potential application? Check out these helpful resources: ADS129x BIOFAQ | ECG Online Training
In reply to Ryan Andrews:
Hello Ryan,
I see. I will ask you by new thread when they have any specific question.
Thank you again and best regards,