Part Number: ADS1018-Q1
Other Parts Discussed in Thread: ADS1015
Hello!
I have a question regarding the ADS1018-Q1 A/D converter.
Usually, the full-scale voltage of the A/D converter is limited by the reference source voltage.
But, in case of ADS1018-Q1 chip, there is no information about what an actual voltage of the internal reference source is.
There is a Full-Scale Range parameter which can be programmed for some different values, for example +/- 1024mV, +/- 2048mV, +/- 6144mV, …
If I choose using +/- 2048mV FSR value and provide power supply voltage of +3.3V, then what is a maximum input analog voltage that can be measured in linear range - 2048mV or 3300mV?
If my power supply voltage is +3.3V and I configure the FSR to +/- 4096mV range, what is a maximal input voltage that can be read without clamping?
Could you please explain this?
Thanks in advance!
Edward Mirodin