Other Parts Discussed in Thread: DAC80504,
Hello!
I used DAC80504 for one of my project is it was working just fine. In this new project I need more channel that is why I chose "same" component with more channels.
Since I could use DAC80504 wihtout any problem and it should be same same so i am assuming I am doing right thing however there is something extra I need to do and I am missing that.
With this new DAC (DAC80508) I can turn on and off the internal reference. But no matter what I write on any channel output the voltage is till 0V.
I am sending the data as 8-bits packages and start with configuring of the GAIN register as (0x04 0x01 0xFF)
Then I write for example to the channel_0 the same way (the first 8-bits 0x08 and then the data in two 8-bits sets).
This communication works perfectly on the DAC80504. I am suspecting that I need to use other registers like SYNC or something else or the output needs a trigger that need to configured through some registers?
Thanks!