Other Parts Discussed in Thread: ADS1292
I have two ads1292RS.They use the same SPI bus and different CLK,CS and DRDY. Both of them use the internal clock. We set both chips at 250SPS continous sample but found one chip will pause(no DRDY signal) about 50ms a t every 2s, at the same time ,the oher chip alwways stopabout 50ms after 4-5 samples. Following the manual,when using the same spi BUS, the Clock PIN should be connect,if we don't connect
these two pin, can the chip work correctly?