Other Parts Discussed in Thread: DAC38J82, DAC37J82, DAC39J84, DAC37J84, DAC38J84
Copied below is para 7.3.11 for the DAC37/38J82 and DAC39J82 DACs. The former have 2 full complex mixers, whereas the DAC39J82 has only one. Is this correct?
I need to generate two analog outputs, < 1M bandwidth, center freq =70+/-2.5MHz. I need two independent NCOs/ complex mixer up-converter. If I read the DAC39J82 data sheet correctly, it cannot do the job I need. Is this correct?
7.3.11 Full Complex Mixer
The DAC37J82/DAC38J82 has two full complex mixer (FMIX) blocks with independent Numerically Controlled
Oscillators (NCO) that enables flexible frequency placement without imposing additional limitations in the signal
bandwidth.
7.3.11 Full Complex Mixer
The DAC39J82 has a full complex mixer (FMIX) block with a Numerically Controlled Oscillator (NCO) that
enables flexible frequency placement without imposing additional limitations in the signal bandwidth. The NCO
has a 48-bit frequency register (phaseaddab (47:0)) and 16-bit phase register (phaseoffsetab (15:0)) that
generate the sine and cosine terms for the complex mixing