Hi,
This is a general ADC question concerning synchronization of system clocks and ADC measurements.
In the old product I am currently converting to a modern MCU, the step up regulator clock (333.333 kHz) is derived from the MCU and LCD display controller clock (8 MHz). The ADS1256 is clocked from a dedicated 7.68 MHz crystal that is not synchronized to the other clocks. According to the designer of the old hardware, these frequencies were carefully chosen (possibly together with the 1000 SPS data rate) for low interference. To me it sounds reasonable to believe that this could be the case, but I currently have little experience in this area. The SYNC#/PDWN# pin is tied HIGH.
With the modern 120 MHz MCU, there is now the possibility of interconnecting timers so that all of the above is synchronized, down to generation of SYNC#/PDWN# pin pulses in phase with ADS1256 XTAL1/CKLIN.
In my particular case, 7.5 MHz and 10 MHz ADS1256 clock frequencies 'work out with the rest'.
Strictly speaking, not all of the timers have to be in phase, as the master timer is either a prescaler or a 'gate controller' to the three slaves that can be started at another counter value than 0. (ADS1256 CLKIN and SYNC#/PDWN# must be in phase in order for timing requirements to be met).
In other words, I have already checked that it _can_ be done (with LCD at 60 MHz and step up regulator clock at 312.5 kHz), but is it a good idea to do it? (Synchronizing all of the above.)
---
Alternatively, it is possible to interconnect two timers that generate LCD display clock and step up regulator clock in phase with each other _and_ two timers that generate ADS1256 CLKIN and SYNC#/PDWN# in phase with each other. These two pairs of interconnected timers are two independent timer pairs. The benefit would be greater flexibility and more viable frequencies compared to the first alternative.
---
I understand that this is potentially a very complex question and that it may be situation-specific, but please see what you can do.
Please don't focus on the particular frequencies. The advice I am seeking is on a conceptual level. (How) does ADC measurements benefit from synchronization with other/all parts of the system?
Thank you and best regards
Niclas