This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSC2046: ADS7846 ADC value

Part Number: TSC2046
Other Parts Discussed in Thread: ADS7846, , AM3352,

I have two question about ADS7846 ADC value

1) I connect Vcc & Vref pin to +3.3V, and measure the voltage of X+,Y+,X-,Y- without touching screen.

    X+ =2.5V

    Y+ =2.5V

    X- =0V

    Y-=0V

   Is that right? Should X+ and Y+ be 3.3V?

2) I get the ADC value of 4 corners but the value is not expected to be close to 0 or 4096.

    What's wrong with this condition? 

    Does this condition lead to the wrong calibration?

    Now I face the wrong calibration and don't put any capacitor or resistance on the X+,Y+,X-,Y- line.

    Right and top (3205,3148)

    Right and bottom (3081,846)

    Left  and top (763,2960)

    Left and bottom (928,1078)