Hi,
I'm designing the ADS1262 into a new project. I want to take advantage of the benefits of CHOP mode, but as I'm planning to bypass the PGA for all inputs, I wanted to be sure I can use this mode. The source of my confusion is section 9.4.12 of the datasheet, which says "The device uses a chopper-stabilized PGA and modulator..." This makes it sound like the chopping circuitry is baked into the PGA itself.
However, in figure 120 just below this paragraph, the chopping circuit is depicted as a discrete block that appears to be separate from the PGA. The bypass switches aren't shown in this diagram, so I'm unsure of where they are relative to the chopping circuit. In looking through the registers, the CHOP enable doesn't seem to have any dependency I can see on enabling the PGA, so I'm hopeful I can set things up the way I'd like.
I'd be grateful for a confirmation from TI before moving forward.
Thanks,
Josh