Part Number: ADS131E04
Other Parts Discussed in Thread: ADS131M04
Hi,
I want to clarify some points regarding my input signal to ADS131E04.
ADS131E04 has a supply voltage of AVDD = 3.3 V and AVSS = 0 V. VREF is set to 2.4 V internal.
Assuming gain is set to 1, am I right that INxP is allowed to be in range from 0 to 2.4 V while INxN is fixed to 0 V? Or is the input range 0.8 V to 2.5 V? How does it look like for gain = 2? 0 V to 1.2 V or 1.3 V to 2 V?
My "signal_single_ended" is conditioned to be in the range of 0 V to 2.4 V. Is it possible to convert the signal with a circuitry as simple as shown above? If not, how should I connect to my signal with the range 0 V to 2.4 V?
Is it possible to connect a single ended signal with the range of 0 V to 3.3 V directly and convert full scale?
Thanks very much.
Regards, Marko