Hello,
I am considering TLA2528 for a new design because it has separate AVDD and DVDD supplies.
On this topic, datasheet says:
AVDD > 2.35V
DVDD > 1.65V
However, later in the doc it is mentioned that input voltage is limited to DVDD (from ESD protection apparently). I found a forum question which suggest using TLA2528 because it would work with AVDD > DVDD.
Could someone confirm if the datasheet is right or if it is an error and it can be used with AVDD=3.6V annd DVDD=1.8V ?