Other Parts Discussed in Thread: THS4521, THS4561, THS4551
We're looking to design an ADS1278 into our monitoring system. We haven't worked with the ADS1278 before. We have in mind to use High Speed mode.
Data sheet (SBAS367F) p. 37 (Application Information) and Figs 88-89 seem to assume that we will use an input buffer. We would like to connect the sensor directly to the differential inputs, without any amplifier in between.
The signal level is roughly 1V(p-p) so we don't need any gain. Our input's impedance will be <200 Ohms. Based on Fig 69, I estimate the ADS1278 effective impedance is about 10kOhm (Fclk=37MHz, so Fmod=~9MHz). It seems as though our sensor should be able to keep up with the current requirements.
So I'd like to ask here: Is there a reason we can't/shouldn't omit the buffer amp between our sensor and the ADS1278 inputs?