Hi team,
I am trying to generate an internal DACCLK with a frequency of 2211.84MHz with the PLL and VCO of the DAC38J84.
I input 122.88MHz externally. N divider=1 / Prescalar=2 /M divider=18, VCO Frequency = 4423.68MHz ( pll_vcosel = '1', pll_vco = '110010'(50), pll_vcoitune = '10 ').
DACCLK frequency should be set to 2211.84 MHz, correct?
Also, is there a frequency range that PFD can be compared to?I guess it depends on the CP value.
Best regards,
Itoh