Other Parts Discussed in Thread: ADS1299
Hello Team TI,
Question 1:
We have received the Evaluation board for ADS1299. However we could not find any probe/ simulator to test the signal.
What testing accessories would be required to test the same?
Do I need to order some probes? If yes, what type of probes does TI suggest for evaluation?
If probes cannot be used, can TI suggest some other testing accessories?
Question 2:
We are exploring active electrodes to use along with the ADS 1299 IC.
Having said that, I am aware that we won't be able to use the internal feature of current source for the lead off detection.
So, the plan is to use an external voltage source that will source the required current in nA.
Even though it is possible to use a current limiter resistor and measure the voltage drop across the resistor to find the current that is flowing to the body. I would like to measure the current in nA through an equipment.
The traditional multimeters are not capable of measuring such a low amount of current. Can TI suggest any equipment/ meter to measure the current?