Hi, I'm testing the respiration function of ADS1292R on our board. The schematic of respiration is same with TI demonstration kit.
AVDD=2.5V and AVSS= - 2.5V
ADS1292R register setting is:
ADS1x9xR_Default_Register_Settings[15] = {
//Device ID read Ony
0x73,
// Device ID read only
//CONFIG1
0x04,
//2000 sps @config 1
//CONFIG2
0xB0,
//4.03V reference, reference buffer enabled @config2
//LOFF
0x10,
// @loff control register
//CH1SET
0x00,
//gain 6 normal operation @ch1set
//CH2SET
0x00,
//gain 6 normal operation @ch2set
//RLD_SENS
0x2C,
//@rld_sens
//LOFF_SENS
0x00,
//loff disabled @loff sens
//LOFF_STAT
0x00,
//@loff_stat
//RESP1
0xCA,
//resp ciruit mod/demod on @resp1
//RESP2
0x03,
//@resp2
//GPIO
0x0C
};
When I test it on the patient (I'm the patient since I do not have patient simulator),
Channel 2 is connected to RA and LA for ECG. Channel 1 is for respiration and share the electrodes with channel 2.
I can get the respiration waveform as this:
seems the function of respiration is good.
But when I change the register setting of Respiration phase RESP_PH[3:0] , there is no obvious difference on the AC portion of the respiration waveform.
the only difference is the DC of the waveform. DC voltage of the waveform increase from 15mV to 49.3mV when Respiration phase RESP_PH[3:0] change from 0000 to 1111.
so it looks fine regardless how RESP_PH[3:0] is configured.
My question are:
1: whether the DC voltage increasing by changing Respiration phase setting is expected? If possible, could you please help explain the theory behind it?
2: Is there any criteria that I can use to evaluate the setting of Respiration phase RESP_PH[3:0]?
Thanks.