Hellow
Model:DAC161S997
1.I want to know the response time of current Loop
I have confirmed in the data sheet that the settling time changes depending on the capacity.
I think the response time will change depending on capacity.
I want to define the change time for current loop from 10% - 90%
2.Is there a maximum output update rate to maintain 4mA current?
Even if the data is continuously updated at 10MHz clock, is the supply current very low?
Please give me advice.